Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: BOOSTXL-DRV8305EVM
Tool/software:
Hi,
I'm currently developing a control algorithm for a PMSM.
I'm using the F28379 Launchpad and the BOOSTXL-DRV8305EVM.
To model the algorithm, I'm using the Microcontroller Blockset in Simulink.
I generate the three dutycycle commands for the three phases and use the ePWM blocks from the blockset in the following.
For the algorithm I'm also including a safestate, where all 6 switches of the inverter should be switched off.
How can I do this while maintaining the ePWM blocks as "connection" to the hardware?
Just requesting a voltage vector with amplitude = 0 in the alpha-beta-system obviously doesn't work,
since this will lead all 3 highsides switched on or all lowsides being switched on (space vector 0/7).