Part Number: TMS320F2800157
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG, OPA350
Tool/software:
Hello,
I am using TMS320F2800157 controller, 32 package
I am using the example (adc_ex10_multiple_soc_epwm) to measure voltage. For ADC counts corresponding to voltages below 15 volts, the error percentage is low. However, as the voltage exceeds 15 volts, the error percentage increases non-linearly.
Its reference voltage is 3.3v internal
The table below presents the measured samples:
| Actual volt(applied volts) | ADC count | Measured volt | Difference voltage |
| 5 | 292 | 4.93 | 0.07 |
| 10 | 585 | 9.89 | 0.109999999999999 |
| 15 | 863 | 14.83 | 0.17 |
| 20 | 1129 | 18.8 | 1.2 |
| 25 | 1390 | 22.9 | 2.1 |
| 30 | 1564 | 26.1 | 3.9 |
| 35 | 1669 | 28.9 | 6.1 |
| 40 | 1767 | 30.9 | 9.1 |
| 45 | 1873 | 31.4 | 13.6 |
| 50 | 1950 | 32.8 | 17.2 |
Could you offer some guidance on how to resolve this issue?
Thanks
Siva Kumar