This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
I have tried to use Math tables in CLA ROM for CLA math operations. I have included the CLA math libraries "cla2_math_library_datarom_fpu32_eabi.lib" and "f28P65xCPU1_CLADATAROM_Symbols_fpu32.lib" as explained in the "CLA Math Library User Guide". But running the program throws warning messages "warning #17003-D: relocation to symbol "_main" overflowed; the 18-bit relocated address 0x23a21 is too large to encode in the 16-bit field (type = 'R_RELWORD' (16), file = "x.obj", offset = 0x00000000, section = ".data")"
Hello - there is an issue with the symbol library for CLA on this device. Please try the attached.