Tool/software:
Hi,
I am trying to understand how to use DAC of the F28379D LaunchXL.
From the device overview document, I can see that DAC A and DAC B are in J3 an J7 as given below:
- DAC OUT A is in MCU pin number 43, Also ADCINA0, J3 Pin 30 of LaunchXL development board
- DAC OUT B is in MCU pin number 42, Also ADCINA1, J7 Pin 70 of LaunchXL development board
- DAC OUT C is in MCU pin number 47, Also ADCINB1
1) DAC A and B are accessible in the dev board. How to access DAC C, which is in pin number 47 of the MCU?
2) Are there examples of how to use the PWM based DAC of the DAC? The file "buffdac_ex1_enable.c" in the driverlib examples folder shows how to use DAC A , not the pwm based DACs.
Thank you for your time.