This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Known good XDS200 stopped working with TMS320F28379D control card

Guru 20045 points
Part Number: TMS320F28379D
Other Parts Discussed in Thread: AM1802

Tool/software:

Hello, 

I have a working XDS200, which is able to connect and debug a TMS320F28355.  Also, it worked with a TMS320F28379D control card until several weeks ago.  Since then I have been using the TMS320F2837D control card's XDS100v2.  I have tried several cables to get it work.  Also, I measured 3.3V on the XDS200's VCC pin.

The results from Test Connection and Debug Connection are shown below. 

Update: I also executed the following command as mentioned in another post

C:\ti\ccs1210\ccs\ccs_base\common\uscif\xds2xx>xds2xx_conf get xds2xxu 0
Error : Failed to open port connection : xds2xxu : 0x0
Error : test failed

Stephen

Debug Connection:

Test Connection:

[Start: Texas Instruments XDS2xx USB Debug Probe_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\s1\AppData\Local\TEXASI~1\
CCS\ccs1210\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
E_RPCENV_IO_ERROR(-6) No connection
Failed to open i/o connection (xds2xxu:0)

An error occurred while soft opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.

The explanation is:
An attempt to access the debug probe via USCIF ECOM has failed.

[End: Texas Instruments XDS2xx USB Debug Probe_0]