This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: ePWM PWM output configured question

Part Number: TMS320F280049
Other Parts Discussed in Thread: C2000WARE

Tool/software:

Dears,

  Customer have some question for ePWM/HRPWM, could you pls help? Thanks. 

1.Can 6 PWM channels be configured as completely independent control instead of complementary output.

2.Can it be configured such that the high side output of phase A are 50% open, and the low side output of phase B and phase C are 50% staggered together (such as one 20% open, one 30% open, two phases staggered)