Tool/software:
Greetings,
Spruii0e section 9.3.3, Figure 9-9 shows that the signals CLBx_OUTy are derived from OUTLUT0-OUTLUT7. But section 9.4.6, Figure 9-18 shows CLBx_OUTy as being the output of the AOC with the OUTLUTy being the input to the AOC. So I’m confused as to which is correct or if Figure 9-9 inadvertently omitted the AOC. Of course, this raises the question of what the source is for CLBx_OUTy in Table 17-5 Output X-BAR Mux Configuration Table etc.
What am I missing?
Thank you,
Ed