Tool/software:
Hello Team,
Could you please help me to implement the ABZ+PWM encoder motor in UMC?
1)First I enabled MOTOR1_ENC, CMD_CAP_EN
2) After enable the CMD_CAP_EN build failed so defined the MACROS #define MTR1_CAP_IDLE_LEVEL 0 in hal.h
3)Do we need to add anything in the code further?
Please need your input to process this further and make UMC to support in ABZ+PWM Encoder.
Thanks
Regards
Shankar Prabhakaran