Hello,
can I use C2000 XDS510LC USB JTAG (spectrum digital) emulator to debug TMS320F28023PT?
A few months ago I used this emulator with TMS320F28335 without any problem. In my actual project I have designed a board with TMS320F28023PT and always getting the following error:
Error connecting to the target:
Error 0x80000200/-140
Fatal Error during: OCS,
Error generated by SD scan controller module
Could that be a driver problem?
I suppose that there is something wrong in general cause I have measured that the XRS is going down each 12ms for about 50µs. I am using an external 12MHz 3,3V Oscillator (same as in my last project) on pin GPIO38 (XCLKIN) and connected X1 to GND and leave X2 open. The TRST is pulled down through 2k2 and EMU0/EMU1 pulled high with 4k7 (datasheet 6.6 Emulator connection without signal buffering for the MCU).
Does anyone can help?