Part Number: TMS320F28379D
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
When programming a TMS320F28379D through Uniflash I am getting the following Error. This happens when I try to Erase Flash as well. I have done multiple power cycles on this board but with no success. The only way I can reprogram the board is if I run the uniflash command line commands then I can reprogram 50% of the time. This is the error I am getting: