Part Number: TMS320F28069
Tool/software:
When using several pins as a simple input and enabling the internal Pull Up, the input always reads as pulled up. I tried a stiff 2K pull down and the input still read high. I disable the pull up and I can read a low when pulled down externally and read a one when pulled up externally. What is the issue with the internal Pull up. I would think I could use it as a normal pull up. My current circuit does not have the external pull up, So I was hoping to use the internal pull up.
Thanks!