Part Number: TMS320F28388D
Tool/software:
When I start my F28388 project without debugger, I keep CPU2 and CM in reset until CPU1 starts CPU2 and CM using Device_bootCPU2() and Device_bootCM().
This allows me to assign IOs, peripherals and memory to each CPU before CPU2 and CM start.
When I use the debugger, the chip behaves differently. When I hit the play button the CPU2 and/or CM start independently and run no matter if CPU1 allows this or not.
This way they try to access memory or peripherals that are not yet available.
Is there a way to configure the debug-configuration such that CPU2 and CM stop and wait until CPU1 starts when the debugger is connected?
Thanks,
Flurin