Part Number: C2000WARE
Tool/software:
Hello
I am facing an issue to generate a2l file with elf file as input.
Elf file is generated with CodeComposerStudio and C2000 compiler v22.6.1
If I load elf file in ASAP2 Studio (from Vector) to generate a2L file I can see that addresses are different compare to .map file. In fact they are *2:
From .map file

From .out file (elf) loaded from ASPA2Studio:

When I use debugger, addresses are conform with .map file.
I was wondering if this was a known issue or if it can be due to bad settings during build.
Thanks for your support,
BR
Vérane Le Rouzic