This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: TMS320F28379D

Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: POWERSUITE, PMP23338, C2000WARE, TMS320F28379D, PMP23069

Tool/software:

Hai,

I'm using LAUNCHXL-F28379D for customization. How to customise the initialization of the example project to initialise all the PWM, GPIO, DAC and ADC pins for our application. Can anyone provide any guide to powersuite customization.

  • Hi Sandra,

    Can you provide more details on what you are trying to do? How does your intended application differ from the software example you are using?

    Thank you,
    Luke

  • I am trying to customise a 10-kW single phase PFC using the ref board.

    I am directly trying to use F280039 example project “3-kW single-phase totem-pole bridgeless PFC with 16-A maximum input Reference design” in PMP23338 folder in C2000Ware powersuite.

     I know the headers are different in submodules but how can I fix it? Can you explain what to do to customise the example to our board i.e TMS320F28379D.

    I appreciate if there is any help. I don't feed any input and not connecting any jumper wires. I was just trying to run the project first.    

  • Hello Sandra

    One way is to start with epwm example project of F28379D in C2000ware. Once it is running, try importing the project file of pmp23338 in this project.

    Better than C2000ware project, you can refer TIDM HV DC-AC (implemented both on F28379D and F28004x) and pmp23069 (implemented on both F28004x and F28003x). Start with TIDM HV DC-AC, F28379D version then import project files from pmp23069. pmp23069 and pmp23338 projects are almost the same except pmp23338 has SDFM based current sensing.

    Thank you

    Amir Hussain