Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hi all,
I have with TMS320F28P650DK9 C2000Ware_5_01_00_00.
I am trying to include the CLAmath.h in the CLA; however, the following line
#define tanf(m) (CLAsin_inline(m)/CLAcos_inline(m))
creates the following compilation error:
>> Compilation failure
source/subdir_rules.mk:16: recipe for target 'source/claTask.obj' failed
"C:/ti/ccs1260/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/include/math.h", line 387: error #18: expected a ")"
Line 387 in math.h is the following line:
_CODE_ACCESS float tanf(float x);
Commenting it out everything works fine.
Any clues?