Part Number: TMS320F28035-EP
Tool/software:
Hello everyone,
I am trying to code my string MPPT boost converter. Nevertheless, I am having difficulty to read the value from ADC and I am getting the follwing error. But there is no problem in tuning while I work with TI reference design. Can anybody help me to resolve this error?
C28xx: Trouble Halting Target CPU: (Error -154 @ 0x0) One of the FTDI driver functions used to write data returned bad status or an error. (Emulation package 9.10.0.00080)
C28xx: Unable to determine target status after 20 attempts
C28xx: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
The error comes only when I turn on power stage. Plus, the CCS gets startled to read any instuctions, including a muse click. After referring the CCS forum, I installed all the drivers for emultion package recommended form TI website; but was not succesfull. Having suspected the EMI issue, the controller is completely isolated with EMI tape, still couldnt be succesfull, can anyone help me out here?
Once I turn on Power stage, all my serial ports are having some commincation issues, because, the wireless mouse even gets non-operatable while I turn on. Just thought of sharing this, in case it could give some suggestion.
Many thanks,
Dr.Ram