Part Number: TPS65219EVM-SKT
Other Parts Discussed in Thread: TPS65219EVM
Tool/software:
Hello, i have a problem with the TPS65219EVM-SKT, we also have the eval kit. I don't know in which forum i should post this issue, so please tell me if the one i choose is incorrect.
So about the problem, we sucessfully configured the voltages with the GUI, without load
But when we add resistors on Vbuck 1 0.44 Ohm with 0.85V and Vbuck 2 0.66 Ohm with 1.1V, and we turn on the alimentation.
The nSTROUT blinks endlessly, and the nINT led turns red, probably meaning theres an error, i don't know why it does that, as we do not overcharge the component.
We also don't give more Ampers than the limit the component can withstand.