This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800157-Q1: TMS32F2800157

Part Number: TMS320F2800157-Q1

Tool/software:

Hello Team,

I'm working on PMSM motor with ABZ+PWM encode.  I am using the TI Universal motor code (UMC) and I have enabled the macros related to the motor encoder. 

Following macros are I enabled "MOTOR1_ENC" on the UMC code.

I'm Checking the eQEP calculated angle & speed. When running the motor there are is no changes on the eQEP calculated angle & speed.

motor_numEncSlots
RsOnLine_pole_rps
RsOnLine_angleDelta_rad 

EST_getAngle_pu
ENC_getElecAngle

speedENC_Hz
angleENC_rad

Thanks,

Regards,

Premkumar.T