Part Number: TMS320F28P650DH
Other Parts Discussed in Thread: ADS8588H, C2000WARE
Tool/software:
Hi Champs,
Customer now want to use TMS320f28P65x to retrieve from ADS8588H, it will need 2 SPI on F28P65x to received data from ADC8588H(DOUTA and DOUTB).

Now customer want to quickly check is it possible to generate CLK and NSS with one SPI, two SPI receive data at the same time, and then read the value of the two SPI fifos with the receive fifo interrupt trigger of one of the SPI? And if it is possible do we have such a example?
Thanks!
Julia