Part Number: TMS320F28069
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hi,
I am looking forward to do a project that has a flash kernal and the application both can be stored in the Flash at the same time. when mcu is needed to be updated the flash kernal will be called to RAM and execute and update the application program through CAN communication. I am required to know the best method to complete this project. I went through both f28069_can_flash_kernal and Example_f2806xFlashProgramming example projects given ion the c2000ware. The problem is that the can_flash_kernal example only executes in the RAM and do not include a Flash section to keep it permanantly. Hope to have further guidance on this.
Thank you,
Best Regards,
Ashan