This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280200DAS



Dear Help desk,

 

I check on the datasheet page 78 of 127 the operation temperature of the CPU around -40°C-125°C depend on package.

 

My customer currently project in normal ambient temperature 25°C and it is working at around 80°C. But for the final product the normal temperature is at 45°C, 20°C higher than prototype build condition, so the correlation of the temperature will be 100°C, it is normal? Do you have any suggestion?  May I know will it effect to CPU life period?

 

Thanks,

Joy

 

  • Can you please clarify your question to better help you.

     

    As the datasheet suggests, the devices (with correct packages) are completely functional from -40'C to 125'C. Based on temperature you mentioned, I don't see any issues.

     

    -Manoj

     

     

  • Dear Manoj,

    If you refer to datasheet, there have a specific temperature for each function we apply to the MCU.

    If we sum all function together and check the temperature totally different than a spec, our temperature higher than state in the datasheet. in fact if at ambient temperature 25°C we already have 80°C for MCU.

    My Customer is doing a Solar microinverter project, the temperature of the MCU will be very high if it is stay at the roof top?

    Can you pls advise base on our customer concern?

    Thanks,Joy

  • When you run your application code at 25'C how did you folks find out that the MCU is already at 80'C? 

    -Manoj