This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280037: Data is being written to auto-generated file warning

Part Number: TMS320F280037

Tool/software:

I am getting the "Data is being written to auto-generated file" warning from the C2000 Hex utility running out of CCS 22.6.0 for a TMS320F280037 MCU.  I have read the forum posts that explain this warning is typically caused by an initialized section on PAGE 1, which suggests an error in the linker command file.  I have reviewed my linker command file closely and there is no mention of PAGE 1 in it.  I have also looked at the .map file that is generated.  Everything seems to be associated with PAGE 0.  I don't see anything about PAGE 1 (I do see a couple of things associated with "abs" for a page number but based on other posts I have read that seems to be ok).

Given that PAGE 1 does not seem to be the issue here, does anybody know what might be causing this warning to be reported?

Thanks,

Jason