Part Number: TMS320F280049C
Other Parts Discussed in Thread: TIDM-1000
Tool/software:
I have two projects: Project One, which I created myself, and Project Two, which is the TI Solution TIDM-1000 (pfc3phvienna).
When I run the same source code in these projects with a 10kHz timer ISR interrupt, Project One has an execution time of 140ns, while Project Two has an execution time of 30ns.
Why is there a difference in execution time between the two projects? Does the TI solution have special settings to optimize execution time?