This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069F: InstaSpin - Torque is really low at low speeds

Part Number: TMS320F28069F

Tool/software:

Hello,

I'm working on a project using InstaSpin FOC, based heavily on the DRV8301-HC-EVM Rev D Eval kit.

It's for an Electric Dental Handpiece, so I need the speed to go from 100 rpm to 40,000 rpm.

The speed isn't an issue currently, but the torque at the low end is almost nonexistent.

At 100 rpm to 500 rpm, all I have to do is touch the motor shaft and it stops.

At the high end, I can't stop it with bare hands at all. I'd have to use needle-nose pliers.

I thought electric motors were supposed to have MORE torque at low speeds.

What's going on here?

Thanks,

Dave