Part Number: TMS320F280025C
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hello.

Now, I am using the XDS110 and trying to write software to TMS320F280025C. But I can't do that. The configuration is shown in the TMS320F280025C data sheet P76 Figure 7-17 and is connected by a TI Legacy 14-pin (TI14). The XDS110 LED is glowing green and not red.
In addition, the error code at the time of writing is "Error-2131@0x0". We must hurry up the development of products with TMS320F280025C.
Thank you in advance.
----------------------------------Below is the full error----------------------------------
IcePick_C_0: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 12.7.0.00105)