Part Number: TMS320F28379D
Other Parts Discussed in Thread: DESIGNDRIVE, CONTROLSUITE, C2000WARE,
Tool/software:
I'm having a lot of trouble with version dependences between the Slave Stack Code Tool and TI's support packages.
I am using a F2837xD chip. After a lot of research and experimentation I have found that I'm required to use: Slave Stack Code Tool v5.11, TI Control Suite and DesignDrive.
The problem with this configuration is that TI ControlSuite is now deprecated (DesignDrive too?) and the Slave Stack Code Tool is now up to v5.13. I was told v5.11 is very old and has some issues that have since been resolved.
If I were using the F2838x micro, I would have support in C2000Ware and at least the newer more stable output of SSC Tool v5.12.
Am I missing something? The TMS320F28379D is still in production.. where is the project for SSC Tool >=5.12 as well as the C2000Ware HAL?