Part Number: TMS320F2800157
Tool/software:
Hi Team,
I am working with TMS320F2800157, 48 Pin Package.
My setup is that a DC voltage supply of 0V to 50V getting converted to 0 to 3.3V using a voltage divider.
This 0 to 3.3V voltage value is getting measured using an ADC on board.
The issue is that there is a variable offset coming when the value is getting measured by the ADC.
The offset increases with the increase in the supply voltage.
I have set the Voltage reference as external reference of 3.3V.
My question is how can we adjust the reading for the ADC and remove the variable offset?