Part Number: TMS320F28384D
Tool/software:
Hi,
I believe spruii0f is the latest tech ref manual for the 2838x family. In Table 28-5, there are no options to use the SOCB of any ePWM. Instead, according to the table there are two options for each EPWM number and both use SOCA. e.g. according to the table a register value of 0 or 1 both give the same Sync Source -> EPWM1_SOCA. Is this correct? Or does a register value of 1 actually set the Sync Source as EPWM1_SOCB? And similarly register values of 5, 9, 13 etc. should all be SOCB for that EPWM?

Thanks,
Fearghal Kineavy