Part Number: TMS320F2800132
Other Parts Discussed in Thread: SYSCONFIG, UNIFLASH
Tool/software:
I have following doubts, regarding DCSM module
Based on my understanding, there are several ways to configure the DCSM module:
* Via Debug Configurations: You can set configurations under Debug Configurations > Target > Flash Settings.
* Using the DCSM Tool: This tool provides specific options for configuring the DCSM module.
* Employing UnFlash Settings & Utilities: This method involves using specific utilities for flash settings.
Question 1: If we configure the DCSM module using multiple methods simultaneously, what will be the resulting configuration?
Question 2: I have to use only .out file, and want to disable all other options. Is there any provision to disable other options ?
Question 3: Is it possible to program same Zone Select Block (Say Zone_Select_Block0) multiple times, if we continue same FLASH passwords & JTAG passwords ?
Question 4: Is it possible to unlock the MCU, if we have both the FLASH and JTAG passwords, but do not have the current link pointer?
Question 5: Even if we use the same FLASH and JTAG passwords when moving to the next LINKPOINTER, is it necessary to update the TargetConfiguration JLM passwords as well?
This is because certain digits of CSMPSWD1 and JTAGPSWDL1 change for each Zone_Select_Block