Part Number: TIDM-1000
Other Parts Discussed in Thread: TMDSCNCD28379D,
Tool/software:

Hi,
I am working with TIDM-1000 board using the control board TMDSCNCD28379D, when I am starting with BUILD1 configuration, getting the output as shown below. I didn't do any calibration for Vbus, Vac, Iac etc.Mainly the current went Irms1,2,3 went wrong. When I measured the currents using the clamp meter, the current observed are Irms1=2.5A (gui_Irms1=4.3), Irms2= 0.9A(gui_Irms2=1.4A) and Irms3=1.6(gui_Irms3=3.08A) etc. These are different from the window I have attached. My queries are
1. How to do calibration for Vbus,Vac,Iac etc? can you please explain some link or procedure?
2. Actually, I am testing with 220Vrms,50Hz ac three phase supply, so what are the changes I have to do with the settings which was not explained in design guide?
3. I have used 200ohm load at the output for the above BUILD1 openloop setup, you have suggested 500ohm load, Is it ok?
Can you please assist me in the above problems?
with regards
Athira T P