This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C-Q1: The NMI trigger source of the TMS320F280039 is abnormal.

Part Number: TMS320F280039C-Q1


Tool/software:

Hello, Ti experts.
  I discovered a problem while testing the NMI trigger function of the TMS320F280039C-Q1 chip. As shown in Figure 1, I've added the test_count2 and test_count variables to the NMI_ISR interrupt service function. test_count2 is used to obtain the NMI trigger source. test_count is used to indicate that the NMI interrupt is entered.

  In Figure 2, I put these two variables into the message 0x123 and send out the values of these two variables. test_count is in the eighth byte of the message and test_count2 is in the seventh byte of the message.
  Figure 3 is the packet data I collected. It can be seen from the data that no trigger source was read after entering the NMI interrupt. May I ask what factors trigger the NMI in this case? thank you!!!