Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: LAUNCHXL-F28P65X
Tool/software:
Hi, expert
I am encountering a problem now when using the 16-bit high-precision ADC sampling of the TMS320F28P65 chip. Have you ever faced such a situation?
The problem description is: When I used the demo board(LAUNCHXL-F28P65X) to sample the voltage at both ends of the dry battery, I found that when the sampling configuration of the ADC was set to 16-bit precision single-ended sampling, through the online simulation of CCS, it could be seen that the fluctuation of the sampling value was very large, approximately 200 LSB. However, when I set it to 16-bit precision differential sampling, the fluctuation of the sampling value in the online simulation was very small, only about 20 LSB. Other configurations were the same, and an external ADC reference was used, with a sampling window of 64 and a 1/4 clock divider. So, do you have any ideas about this situation?