Part Number: TMS320F28P659DK-Q1
Tool/software:
Hi,
I have tried the Example codes to oversample an ADC input channel using the trigger repeater block to generate repeated pulses using EPWM1 SOCA as the trigger source, and PPB block to accumulate the sum and average it.
As mentioned in the TRM there is only 4 PPB block per ADC module to calculate the average of accumulated result.
Now, I have to use more than 10 ADC channels per module. In that case, are there any other provisions to use oversampling.
I have also gone through Software oversampling, where multiple SOCs are configured to trigger the same ADC input channels. But that also wont be applicable in my case as i am already configuring 10 SOCs for the 10 input ADC channels.
Thanks in Advance,
Regards,
Rupa