Other Parts Discussed in Thread: C2000WARE, SYSCONFIG
Tool/software:
I am working with the 280039C launchxl board. I have a C:\ti\c2000\C2000Ware_5_02_00_00\driverlib\f28003x\examples\spi working which has a .syscfg file - spi_ex4_external_loopback_fifo_interrupts.syscfg.
I created a new project and wanted to add this .syscfg file. I copied the spi_ex4_external_loopback_fifo_interrupts.syscfg to the new project.
From what I could find this is all I should have to do.
When I open the .syscfg file in the new project I have errors I did not have in the original project.

I do not have this error in the original C2000 SPI project with this bit rate.
Looking at the properties for the C2000 SPI project I see the following:


Where as in the new project I see:


So can you not just copy in a .syscfg file from one project to another?
Brent