This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEMU110-U: Not detect in COM port in PC

Part Number: TMDSEMU110-U

Tool/software:

After purchasing a new XDS110 debug probe from Texas Instruments (TI), I connected it to my PC. Despite installing all the necessary software packages and drivers, the COM port for the XDS110 does not appear on the PC.

Upon connecting the XDS110 debug probe to a C2000 docking station equipped with the TMS320F283788D MCU, I encountered the following error details:

[Start: Texas Instruments XDS110 USB Debug Probe_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\sheik\AppData\Local\TEXASI~1\CCS\
ccs1271\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100/110/510 class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Jul 24 2024'.
The library build time was '18:57:55'.
The library package version is '12.8.0.00189'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.

An error occurred while hard opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-260' (0xfffffefc).
The title is 'SC_ERR_XDS110_OPEN'.

The explanation is:
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the XDS110SupportReadMe.pdf
file there for instructions.

[End: Texas Instruments XDS110 USB Debug Probe_0]

Please help us.