Part Number: TMS320F2812
Tool/software:
Hello:
At present, the two pins XA [15] and XA [16] of the chip circuit are connected to external RAM on the other end. If there is a short circuit, if the DSP program outputs a high level to pin XA [15] and a low level to pin XA [16], and these two pins are short circuited, what is the actual output high? Is it still low? Thanks!!!