This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

breakpoint setting in CCS

http://e2e.ti.com/support/microcontrollers/tms320c2000_32-bit_real-time_mcus/f/171/p/21510/83134.aspx#83134

the post above says:

These breakpoints can be disabled by navigating CCS menu Option -> Customize -> Program/Project/CIO and enabling the two checkboxes titled Do Not Set End of Program Breakpoint At Load and Do Not Set CIO Breakpoint At Load. Close and restart CCS and now you should have access to the 2 breakpoints.

 

in my CCS 4.2.3.00004, there is no such menu:  Option -> Customize,etc,  is this talking about old vertion of CCS?

where can I set this in new CCS?

 

thanks