Part Number: LAUNCHXL-F28P65X
Tool/software:
Hi team
my customer is using F28P65 and they found that when they run with their own software, the temp will raise to 70 degree centigrade in a 25 degree centigrade environment. They are using the external LDO and 6 layers PCB with power and GND layer following the EVM layout.
The board will be put into the control cabinet and the temp will rise to 100 degree centigrade . The worst environment will be up to 50 degree centigrade and they are afraid that the temp of the chip will rise above 125 degree. Do u think it is a high risk?
the hardware is no problem because the system can work well.
i have also let them to test the EVM board with their own software running. It is surprising to find that the chip will rise up to 160 degree centigrade. do u think it makes sense?
could u kindly give some advise?thanks