This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Is there a Tile Enable Signal?

Part Number: TMS320F28379D

Tool/software:

Greetings,

When a CLB tile is enabled, is there any signal which is or can be generated to use inside the tile?

Thank you,

Ed

  • Hi Ed,

    I don't think this signal is accessible from inside the CLB.

    The CLB PSCLK(pre-scaled clock) can be used as an input via the Local Input Mux:

    The CLB clock can be enabled or disabled manually in software.

    You can also create your own enable signal using the GPREG boundary input and customize your TILE configuration to activate when this input is true.

    Thank you,

    Luke

  • Hi Luke,

    Creating my own enable signal was my Plan B.  I will go with that.

    Thank you for looking,

    Ed

  • Hi Ed,

    Sounds good, I will close this thread.

    --Luke