Part Number: TMS320F28377S
Other Parts Discussed in Thread: C2000WARE
Tool/software:
We are familiar and experienced with firmware update of TMS320F28377S via SCI interface. There is good documentation for SCI firmware update and flash kernel is also available. In our next design we are considering to perform firmware update of TMS230F28377S using CAN interface. We have tried searching the TI e2e portal and found that this documentation is the most relevant: SPRAD51A – DECEMBER 2023 – REVISED APRIL 2024 . However this document targets different devices. In this regard we have the following initial queries:
1- Is there a CAN flash kernel available for TMS320F28377S device or we need to modify the CAN flash kernel for TMS320F28003x?. If this is the case then please advise the required changes.
2- Can we use the same host application as the one available for TMS320F28003x?. If no then let us know the required changes.