This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650DK: Important and urgent:The issue of chip heating

Part Number: TMS320F28P650DK

Tool/software:

The TMS320F28P650D NFBGA (NMR) 169pin chip can be used normally but heats up to above 100°. Please help check whether there are problems with the principle and wiring? If not, whether there is a problem with the chip itself. For a similar application, the NFBGA (ZEJ) 256pin chip works fine and does not have this heating problem.