Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hello Team,
I'm trying to establish UART communication on the TMS320F28388D processor using both cores. To achieve this, I've copied below file from C2000Ware_5_02_00_00\libraries\diagnostic\f2838x\examples\test_application.
//#############################################################################
//
// FILE: sta_comm.c
//
// TITLE: Self Test Application Communication source
//
//#############################################################################
// $TI Release: C2000 Diagnostic Library v3.00.00 $
// $Release Date: Tue Oct 19 17:39:05 IST 2021 $
// $Copyright:
// Copyright (C) 2021 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//#############################################################################
//
// Included Files
//
#include "driverlib.h"
#include "device.h"
#include "sta_comm.h"
//*****************************************************************************
//
// STA_Comm_configSCIA(void)
//
//*****************************************************************************
void STA_Comm_configSCIA(void)
{
//
// GPIO28 is the SCI Rx pin.
//
GPIO_setPinConfig(DEVICE_GPIO_CFG_SCIRXDA);
GPIO_setPadConfig(DEVICE_GPIO_PIN_SCIRXDA, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCIRXDA, GPIO_QUAL_ASYNC);
//
// GPIO29 is the SCI Tx pin.
//
GPIO_setPinConfig(DEVICE_GPIO_CFG_SCITXDA);
GPIO_setPadConfig(DEVICE_GPIO_PIN_SCITXDA, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCITXDA, GPIO_QUAL_ASYNC);
//
// Initialize SCIA and its FIFO.
//
SCI_performSoftwareReset(SCIA_BASE);
SCI_setConfig(SCIA_BASE, SysCtl_getLowSpeedClock(DEVICE_OSCSRC_FREQ),
STA_COMM_BAUD_RATE, (SCI_CONFIG_WLEN_8 | SCI_CONFIG_STOP_ONE |
SCI_CONFIG_PAR_NONE));
SCI_resetChannels(SCIA_BASE);
SCI_resetTxFIFO(SCIA_BASE);
SCI_clearInterruptStatus(SCIA_BASE, SCI_INT_TXFF | SCI_INT_RXFF);
SCI_enableFIFO(SCIA_BASE);
SCI_enableModule(SCIA_BASE);
SCI_performSoftwareReset(SCIA_BASE);
}
//*****************************************************************************
//
// STA_Comm_transmitData(unsigned char *msg)
//
//*****************************************************************************
void STA_Comm_transmitData(unsigned char *msg)
{
int16_t i;
i = 0;
while(msg[i] != '\0')
{
SCI_writeCharBlockingFIFO(SCIA_BASE,(uint16_t)msg[i]);
i++;
}
}
//
// STA_Main_configXCLKOut(void)
//
void STA_Main_configXCLKOut(void)
{
// Configure GPIO as SYSCLK out
GPIO_setPadConfig(73, GPIO_PIN_TYPE_STD);
GPIO_setPinConfig(GPIO_73_XCLKOUT);
// Clock source is SYSCLK
SysCtl_selectClockOutSource(SYSCTL_CLOCKOUT_SYSCLK);
EALLOW;
// XCLOCK out = clock source /8
HWREG(CLKCFG_BASE + SYSCTL_O_XCLKOUTDIVSEL) = 3U;
EDIS;
}
//
// End of File
//
The below function is called from main.c. This function is used for debugging.
- STA_Comm_configSCIA();
- STA_Comm_transmitData("Test 1");
I have copied the same code onto both cores. Both cores are running as expected, which I verified by observing the LED blinking pattern. However, UART communication is only being established on core 1, as I am receiving messages from core 1, but I am not observing any messages from core 2.
Also i have initialized the UART on core1 and only STA_Comm_transmitData("Test 1"); used to send data from core 2 without initializing interface again on core2 but no success.
In addition to that I have initialized UART on core 1, I have only called STA_Comm_transmitData("Test 1") from core 2 to send data, without reinitializing the UART interface on core 2, but unfortunately, this approach has not been successful.
Attached core1 and core2 linker files.
Core1 Linker
MEMORY
{
HWBIST : origin = 0x000000, length = 0x000020
/* BEGIN is used for the "boot to Flash" bootloader mode */
BEGIN : origin = 0x080000, length = 0x000002
// BOOT_RSVD : origin = 0x000002, length = 0x0001AF /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x0001B1, length = 0x00024F
RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */
// RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
RAMD0 : origin = 0x00C000, length = 0x000800
RAMD1 : origin = 0x00C800, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800
RAMLS6 : origin = 0x00B000, length = 0x000800
RAMLS7 : origin = 0x00B800, length = 0x000800
RAMGS0 : origin = 0x00D000, length = 0x001000
RAMGS1 : origin = 0x00E000, length = 0x001000
RAMGS2 : origin = 0x00F000, length = 0x001000
RAMGS3 : origin = 0x010000, length = 0x001000
RAMGS4 : origin = 0x011000, length = 0x001000
RAMGS5 : origin = 0x012000, length = 0x001000
RAMGS6 : origin = 0x013000, length = 0x001000
RAMGS7 : origin = 0x014000, length = 0x001000
RAMGS8 : origin = 0x015000, length = 0x001000
RAMGS9 : origin = 0x016000, length = 0x001000
RAMGS10 : origin = 0x017000, length = 0x001000
RAMGS11 : origin = 0x018000, length = 0x001000
RAMGS12 : origin = 0x019000, length = 0x001000
RAMGS13 : origin = 0x01A000, length = 0x001000
RAMGS14 : origin = 0x01B000, length = 0x001000
RAMGS15 : origin = 0x01C000, length = 0x000FF8
// RAMGS15_RSVD : origin = 0x01CFF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
/* Flash sectors */
FLASH0 : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
FLASH1 : origin = 0x082000, length = 0x002000 /* on-chip Flash */
FLASH2 : origin = 0x084000, length = 0x002000 /* on-chip Flash */
FLASH3 : origin = 0x086000, length = 0x002000 /* on-chip Flash */
FLASH4 : origin = 0x088000, length = 0x008000 /* on-chip Flash */
FLASH5 : origin = 0x090000, length = 0x008000 /* on-chip Flash */
FLASH6 : origin = 0x098000, length = 0x008000 /* on-chip Flash */
FLASH7 : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
FLASH8 : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
FLASH9 : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASH10 : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASH11 : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASH12 : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASH13 : origin = 0x0BE000, length = 0x001FF0 /* on-chip Flash */
// FLASH13_RSVD : origin = 0x0BFFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
CPU1TOCPU2RAM : origin = 0x03A000, length = 0x000800
CPU2TOCPU1RAM : origin = 0x03B000, length = 0x000800
CPUTOCMRAM : origin = 0x039000, length = 0x000800
CMTOCPURAM : origin = 0x038000, length = 0x000800
CANA_MSG_RAM : origin = 0x049000, length = 0x000800
CANB_MSG_RAM : origin = 0x04B000, length = 0x000800
RESET : origin = 0x3FFFC0, length = 0x000002
}
SECTIONS
{
codestart : > BEGIN, ALIGN(8)
.text : >> FLASH1 | FLASH2 | FLASH3 | FLASH4, ALIGN(8)
.cinit : > FLASH4, ALIGN(8)
.switch : > FLASH1, ALIGN(8)
.reset : > RESET, TYPE = DSECT /* not used, */
/* HWBIST reset context restore code must be placed at 0x0000 */
hwbist : LOAD = FLASH3,
RUN = HWBIST,
LOAD_START(HwbistLoadStart),
LOAD_SIZE(HwbistLoadSize),
RUN_START(HwbistRunStart),
PAGE = 0, ALIGN(4)
/* Must be placed lower than a 16-bit memory address */
hwbiststack : > RAMM0
.stack : > RAMM1
.init_array : > FLASH1, ALIGN(8)
.bss : > RAMLS5
.bss:output : > RAMLS3
.bss:cio : > RAMLS5
.data : > RAMLS5
.sysmem : > RAMLS5
/* Initalized sections go in Flash */
.const : > FLASH5, ALIGN(8)
ramgs0 : > RAMGS0, type=NOINIT
ramgs1 : > RAMGS1, type=NOINIT
ramm0 : > RAMM0, type=NOINIT
MSGRAM_CPU1_TO_CPU2 : > CPU1TOCPU2RAM, type=NOINIT
MSGRAM_CPU2_TO_CPU1 : > CPU2TOCPU1RAM, type=NOINIT
MSGRAM_CPU_TO_CM : > CPUTOCMRAM, type=NOINIT
MSGRAM_CM_TO_CPU : > CMTOCPURAM, type=NOINIT
/* The following section definition are for SDFM examples */
Filter_RegsFile : > RAMGS0
Filter1_RegsFile : > RAMGS1, fill=0x1111
Filter2_RegsFile : > RAMGS2, fill=0x2222
Filter3_RegsFile : > RAMGS3, fill=0x3333
Filter4_RegsFile : > RAMGS4, fill=0x4444
Difference_RegsFile : >RAMGS5, fill=0x3333
#if defined(__TI_EABI__)
.TI.ramfunc : {} LOAD = FLASH3,
RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
ALIGN(8)
#else
.TI.ramfunc : {} LOAD = FLASH3,
RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
ALIGN(8)
#endif
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
Core2 linker
MEMORY
{
HWBIST : origin = 0x000000, length = 0x000020
/* BEGIN is used for the "boot to Flash" bootloader mode */
BEGIN : origin = 0x080000, length = 0x000002
//BOOT_RSVD : origin = 0x000002, length = 0x0001A7 /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x0001A9, length = 0x000257
RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */
// RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
RAMD0 : origin = 0x00C000, length = 0x000800
RAMD1 : origin = 0x00C800, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800
RAMLS6 : origin = 0x00B000, length = 0x000800
RAMLS7 : origin = 0x00B800, length = 0x000800
RAMGS0 : origin = 0x00D000, length = 0x001000
RAMGS1 : origin = 0x00E000, length = 0x001000
RAMGS2 : origin = 0x00F000, length = 0x001000
RAMGS3 : origin = 0x010000, length = 0x001000
RAMGS4 : origin = 0x011000, length = 0x001000
RAMGS5 : origin = 0x012000, length = 0x001000
RAMGS6 : origin = 0x013000, length = 0x001000
RAMGS7 : origin = 0x014000, length = 0x001000
RAMGS8 : origin = 0x015000, length = 0x001000
RAMGS9 : origin = 0x016000, length = 0x001000
RAMGS10 : origin = 0x017000, length = 0x001000
RAMGS11 : origin = 0x018000, length = 0x001000
RAMGS12 : origin = 0x019000, length = 0x001000
RAMGS13 : origin = 0x01A000, length = 0x001000
RAMGS14 : origin = 0x01B000, length = 0x001000
RAMGS15 : origin = 0x01C000, length = 0x000FF8
// RAMGS15_RSVD : origin = 0x01CFF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
/* Flash sectors */
FLASH0 : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
FLASH1 : origin = 0x082000, length = 0x002000 /* on-chip Flash */
FLASH2 : origin = 0x084000, length = 0x002000 /* on-chip Flash */
FLASH3 : origin = 0x086000, length = 0x002000 /* on-chip Flash */
FLASH4 : origin = 0x088000, length = 0x008000 /* on-chip Flash */
FLASH5 : origin = 0x090000, length = 0x008000 /* on-chip Flash */
FLASH6 : origin = 0x098000, length = 0x008000 /* on-chip Flash */
FLASH7 : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
FLASH8 : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
FLASH9 : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASH10 : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASH11 : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASH12 : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASH13 : origin = 0x0BE000, length = 0x001FF0 /* on-chip Flash */
// FLASH13_RSVD : origin = 0x0BFFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
CPU1TOCPU2RAM : origin = 0x03A000, length = 0x000800
CPU2TOCPU1RAM : origin = 0x03B000, length = 0x000800
CPUTOCMRAM : origin = 0x039000, length = 0x000800
CMTOCPURAM : origin = 0x038000, length = 0x000800
RESET : origin = 0x3FFFC0, length = 0x000002
}
SECTIONS
{
codestart : > BEGIN, ALIGN(8)
.text : >> FLASH1 | FLASH2 | FLASH3 | FLASH4, ALIGN(8)
.cinit : > FLASH1, ALIGN(8)
.switch : > FLASH1, ALIGN(8)
.reset : > RESET, TYPE = DSECT /* not used, */
/* HWBIST reset context restore code must be placed at 0x0000 */
hwbist : LOAD = FLASH4,
RUN = HWBIST,
LOAD_START(HwbistLoadStart),
LOAD_SIZE(HwbistLoadSize),
RUN_START(HwbistRunStart),
PAGE = 0, ALIGN(4)
/* Must be placed lower than a 16-bit memory address */
hwbiststack : > RAMM0
.stack : > RAMM1
#if defined(__TI_EABI__)
.init_array : > FLASH1, ALIGN(8)
.bss : > RAMLS3
.bss:output : > RAMLS3
.bss:cio : > RAMLS3
.data : > RAMLS2
.sysmem : > RAMM1
/* Initalized sections go in Flash */
.const : > FLASH5, ALIGN(8)
#else
.pinit : > FLASH1, ALIGN(8)
.ebss : > RAMLS3
.esysmem : > RAMM1
.cio : > RAMLS3
/* Initalized sections go in Flash */
.econst : >> FLASH4 | FLASH5, ALIGN(8)
#endif
ramgs0 : > RAMGS0, type=NOINIT
ramgs1 : > RAMGS1, type=NOINIT
ramm0 : > RAMM0, type=NOINIT
ramm1 : > RAMM1, type=NOINIT
MSGRAM_CPU1_TO_CPU2 : > CPU1TOCPU2RAM, type=NOINIT
MSGRAM_CPU2_TO_CPU1 : > CPU2TOCPU1RAM, type=NOINIT
MSGRAM_CPU_TO_CM : > CPUTOCMRAM, type=NOINIT
MSGRAM_CM_TO_CPU : > CMTOCPURAM, type=NOINIT
/* The following section definition are for SDFM examples */
Filter_RegsFile : > RAMGS0
Filter1_RegsFile : > RAMGS1, fill=0x1111
Filter2_RegsFile : > RAMGS2, fill=0x2222
Filter3_RegsFile : > RAMGS3, fill=0x3333
Filter4_RegsFile : > RAMGS4, fill=0x4444
Difference_RegsFile : >RAMGS5, fill=0x3333
#if defined(__TI_EABI__)
.TI.ramfunc : {} LOAD = FLASH3,
RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
ALIGN(8)
#else
.TI.ramfunc : {} LOAD = FLASH3,
RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
ALIGN(8)
#endif
/* The following section definition are for DCSM dual core examples */
ZONE1_RAM : > RAMLS4
UNSECURE_RAM : > RAMLS6
CSMKEY_RAM : > RAMD0
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
Thanks & Regards,
Vikram Tathe