This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F2800157: Red light is not blinking

Part Number: LAUNCHXL-F2800157

Tool/software:

I'm using the freertos_ex1_c28x_led_blinky project but i don't see the red led blink at all when running the project (i do see the green led blink). I've tried making a seperate c file to test that i can blink the individual leds and i'm only able to get led5 (green) to blink. If i unplug and plug back in the launchpad i am able to see led 4 (red) blink but not when i tried to blink it through the code. When i look through the schematic the led mapping looks correct (led1 is on 35u and led2 is on 49u. Not sure why i can't get led4 to blink. Any help/insight would be great.

Thanks