Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE
Tool/software:
Trying to add an sysconfig of an example code from driverlib from c2000 ver 5-01-00 but it is showing error of missing device or board. And if I am taking from the training example of control configuration file is loaded.. What is the issue please help.
2. I was trying to generate 3 pulses with a phase shift of 120 degree and duty cycle of 30% but unable to implement. If I am using phase shift count value it is not working properly through syscong? please example this why through sysconfig file unable to generate pulses properply there is an uneven gaps between pulses which is not desired