Part Number: TMS320F2800137
Other Parts Discussed in Thread: C2000WARE
Tool/software:
The Ld and Lq of IPMSM (Inner-mounted Permanent Magnet Synchronous Motor) are different, but the values of Ld and Lq are the same in the motor parameters learned by C2000Ware MotorControl SDK. I have the following questions:
1. Can the FAST observer in C2000Ware MotorControl SDK be used to control IPMSM?
2. Can the learned motor parameters be directly filled into user_mtr1.h? Will this cause abnormal motor control?
3. Why is the three-phase current waveform of my IPMSM worse when controlled by MTPA than when not controlled by MTPA when using FAST observer?
4.When using the FAST observer, how do I set the motor parameters to correctly control the IPMSM?