Other Parts Discussed in Thread: DRV8353
Tool/software:
Hi,
We are working on a custom board with F2800157 MCU. Same MCU Launchpad with DRV8353 we can run the motor smoothly at various speeds.
But when we moved the code verified code to the custom board, the motor ran for a few minutes and got stopped by the module due to the current error.
1)in the custom board we not using a DRV8353 Chip instead of using an IRF2286 gate driver Is the doubt in the calculation of full-scale current and voltage?
The full-scale voltage we calculated based on the divider resistor but we Full-scale current we don't know for because in DRV8353 using current gain we set
various full-scale current values here no way to adjust the current gain and the current shunt is 0.3 ohm.
As per 0.3 ohms if calculated I got the value as 110 but not sure about the gain in IRF but the gain is adjustable in DRV .How to calculate for IRF ?
2) If some random values for USER_M1_ADC_FULL_SCALE_CURRENT_A behaviors are different motor running for some time and getting the module over the current fault. finally motor stopped.
3) The motor running at 50ns dead band at Build_Level2 without issues, but, the same deadband motor not running at BL#3 and BL#4 . The motor only runs if we set 4000 to 5000 deadband.
Kindly help us, we are sure there are some calculation issues with ADC Full-scale current values.
Appreciate your help asap.
Thanks
Prabhakaran