Hello,
I have a question – concerning the thermal pad of the PFP/PZP packages of the TMS320F28066PFP? Is there any electrical connection recommendation? Should it be left “floating” or be connected to GND?
Also, there appears to be an error in the 2806x datasheet, in the product selection table (section 3.1). For “High Resolution Capture Modules (HRCAP)” it lists “4” for all parts, all packages. Actually, it looks like there is only ONE HRCAP available in the 80pin packages. Is thsi true?
Thanks,
Todd