Part Number: LP-XDS110
Other Parts Discussed in Thread: LAUNCHXL-F280049C, CCSTUDIO
Tool/software:
Installed Code Composer V12.8.0.00012 on new Windows 11 laptop selecting only C2000 real-time MCUs option
Tried to upload program to LAUNCHXL-F280049C which has XDS110 probe with firmware 3.0.0.5 which failed. Error message says probe must be upgraded to firmware version 3.0.0.31. Attempted to update from code composer- FAILED
Tried using windows 10 laptop running Code Composer version 9.1.0.00010, and successfully reprogramed the LAUNCHXL-F280049C i.e. still WORKING
Closed Code Composer on Windows 11 laptop
Attempted to update firmware using XDSDFU program on Windows 11 system running V12,
XDSDFU -e Finds 1 device , version 3.0.0.5
Windows device manager
PORTS: XDS110 Class Application User (COM?), XDS110 Class Auxiliary Data Port (COM?)
Texas Instruments Debug Probes: XDS110 Class Data Port, XDS110 Class Debug Probe
XDSDFU -m Finds device, switches device into DFU mode
Windows Device Manager now shows under other devices :
Tiva Device Firmware Update
Tiva Device Firmware Update properties Drivers not installed
XDSDFU -f filename_3.0.0.31.bin -r
The requested device was not found on the bus
In C:\ti and its sub-folders windows search finds :
No files labelled Tiva
3 files labelled stellaris
stellaris_emu.dvr
C:\ti\ccs1280\ccs\ccs_base\DebugServer\drivers
device_stellaris.xml
C:\ti\ccs1280\ccs\ccs_base\emulation\analysis\xmldb\trace_config\devices
XDS110_StellarisDFU.png
C:\ti\ccs1280\ccs\eclipse\plugins\com.ti.ccstudio.usersguide.doc_12.8.0.202407301400\html\xdsdebugprobes\images
How to I update the firmware on the XDS110 on my board?