Part Number: TMS320F280039C
Tool/software:
Hi team,
The CLA interrupt cannot step through debugging, and its starting address is 0x00, which is not the 0x9000 I defined in the cmd file


At the same time, there will also be the following error messages
CLA1_0: Can't Run Target CPU: (Error -2134 @ 0x0) Unable to control device execution state. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 12.7.0.00130)
But by adding IO judgment in the TASK1 interrupt, it was found that cla TASK1 was running normally.
Could you please clarify my confusion?
Thank you.
Best regards,
Jiahui