This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-02011: setup questions on TIDM-02011

Part Number: TIDM-02011


Tool/software:

Hi Champ,

I am asking for my customer. 

They are referring to our TIDM-02011 to develop LFU w/o reset on F28003x.

After importing into CCS (location : solutions\tidm_02011\f28003x), there are 5 projects. 

(1). Supposed we only need buck_F28003x_lfu as application image, and combining the project flash_kernel_ex3_sci_flash_kernel to implement the all LFU, right ? What is the project buck_kernel_F28003x_lfu used for ?

(2). In project flash_kernel_ex3_sci_flash_kernel, there are many excluded .cmd files (28003x_flash_bank0/1/2_LDFU_lnk) by default, from the TIDM-02011 design guide in 3.4 Test Setup, it didn't mention about any .cmd file to build up with. Asking on what are these .cmd files for ? 

(3). Continue on 2nd question, in practical implementation at customer's side, similar concept on having few .cmd files in a same project folder to determine old / new images to be allocate to the memory ? 

Thanks for the help.

Regards,

Johnny

  • HI Johnny,

    I'm looking into this request and will get back to you shortly.

    Regards,

    Ozino

  • Johnny,

    1. buck_kernel_F28003x_lfu - this is app + kernel combined into one project. Wayne had requested this - some customers ask for this.

    2. Different build configurations use different cmd files. For a specific build configuration, one cmd file will be used and the others excluded.

    3. Didn't quite understand the question. If the question is whether the same structure can be followed even for the customer's project as ours, then yes it can.

    Thanks,

    Sira